Technical FAQs

Ask a Question

What is the temperature rating for the L100/L300limit switch cable10100010 for ?

The temperature rating is 60 deg C. Higher ratings are available in the modified HL100 series.



CTA-ID : 2036702
Was this helpful?
What can we do to improve the information ?