Technical FAQs

Ask a Question

What is the recommended size of the lock shank that can be used on the QO1HPL handle padlock attachment?

Use a 1/8`` to 5/16`` lock shank.


CTA-ID : 2036719
Was this helpful?
What can we do to improve the information ?