Technical FAQs

Ask a Question

What is a NEMA 7 rating for a 9036DR31?

Indoor use in locations classified as Class 1, Division 1, Groups A, B, C or D hazardous locations as defined in the National Electrical Code, NFPA 70, commonly referred to as explosion proof While this product is enclosed, the hazardous rating applies only if there is no gasket around the cover.

For this reason condensation or liquid from washdown can get trapped inside the enclosure and will not drain out.


CTA-ID : 2036665
Was this helpful?
What can we do to improve the information ?