Technical FAQs

Ask a Question

Do the Masterpact OF aux. contacts operate before or after the main contacts?

The OF contacts are linked to the crossbar and switch after the main contacts. The time lag is from 1 ms to 23 ms. The contacts may bounce for up to 70 ms.

CTA-ID : 2036627
Was this helpful?
What can we do to improve the information ?