Technical FAQs

Ask a Question

What does the suffix ``TS`` mean on a the load center, QO24L70TS?

The ``S`` indicates that the load center is available with a surface cover only. It is not available as a flush unit. The `T` indicates the load center has a factory installed ground bar.

CTA-ID : 2036510
Was this helpful?
What can we do to improve the information ?