Technical FAQs

Ask a Question

Are the QO convertible(MB to ML or ML to MB) load centers available in a nonmetallic(Plastic) enclosure?

Issue:
Product Design

Product Line:
QO and Homeline load centers

Environment:
Enclosure material

Cause:
Application

Resolution:
No. Square D does not make any of the QO or Homeline Convertible load centers in a Non-Metallic(or Plastic) enclosure.


CTA-ID : 2036506
Was this helpful?
What can we do to improve the information ?