Technical FAQs

Ask a Question

What is the short circuit current rating for the HOM2040M200TC load center?

Issue:
Application

Product Line:
Homeline LC

Cause:
Application

Resolution:
The short circuit current rating 22K AIR. The main circuit breaker has a "Series Rating" with the branch circuit breakers, and it is referred to as a 22/10 Series Rating The main circuit breaker is rated at 22K AIR, and the branch circuit breakers are 10K AIR.


CTA-ID : 2036499
Was this helpful?
What can we do to improve the information ?