Technical FAQs

Ask a Question

When ordering factory assembled NQ and NF type 2 section panelboards, how do the two panels interconnect from top to bottom?

Issue:
When ordering factory assembled NQ and NF type 2 section panelboards, how do the two panels interconnect from top to bottom? 

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The main breaker panel will feed from top to bottom, which will then feed the bottom of the next main lug only panel. The two panels connect together on the bottom end.


CTA-ID : 2036190
Was this helpful?
What can we do to improve the information ?