Technical FAQs

Ask a Question

Is there an anti-inversion clip for use with an EZML332400?

Yes, order separately and install one catalog number MMLRK per meter socket position to prevent a Class 320 watt-hour meter from being installed upside down (inverted), and also to reject use of a Class 100 or Class 200 watt-hour meters.



CTA-ID : 2036177
Was this helpful?
What can we do to improve the information ?