Technical FAQs

Ask a Question

What is the mounting hole pattern for the base of a XVBL beacon ?

There are 2 x 4.5mm diameter holes with 42mm centerlines outside the 27mm dia center wire hole . This matches the dimension of the XVBC21.


CTA-ID : 2036164
Was this helpful?
What can we do to improve the information ?