Technical FAQs

Ask a Question

Is the EZM32000CB available with a 100% rated main breaker?

This device is available with a 80% rated breaker only.


CTA-ID : 2036500
Was this helpful?
What can we do to improve the information ?