Technical FAQs

Ask a Question

What is the connector for an XMLF***E204* ?

See digest 172 page 18-10 reference 31 or 32 AC/DC 5 pin connector.

6` cable, straight connector, Yellow - XSZCA1501Y
15` cable, straight connector, Yellow - XSZCA1502Y
30` cable, straight connector, Yellow - XSZCA1503Y

6` cable, 90 degree connector, Yellow - XSZCA9501Y
15` cable, 90 degree connector, Yellow - XSZCA9502Y
30` cable, 90 degree connector, Yellow - XSZCA9503Y

Note that all XMLF......E... pressure switches are AC only .


CTA-ID : 2036378
Was this helpful?
What can we do to improve the information ?