Technical FAQs

Ask a Question

What is the maximum voltage under DC current for the OF/SD auxiliary contacts of the C60?

The maximum current and voltage for the C60 SD and OF are 1A, 130VDC


CTA-ID : 2036339
Was this helpful?
What can we do to improve the information ?