Technical FAQs

Ask a Question

What is the torque value for the Phase, Neutral and Equipment Ground Terminal wire binding screws in an EZM3800TB tap box?

The EZM3800TB tap box is supplied with factory installed terminals to accommodate (4) 3/0 AWG to 500 kcmil AL/CU wires per Phase and Neutral and the torque value for all wire sizes in these lugs is listed as 275 inch pounds.
This EZM3800TB tap box is also supplied with a factory installed terminal to accommodate (1) #6 AWG to 300 kcmil AL/CU wire per Equipment Ground Terminal and the torque value for all wire sizes in this lug is also listed as 275 inch pounds.


CTA-ID : 2036434
Was this helpful?
What can we do to improve the information ?