Technical FAQs

Ask a Question

Does the busway fusible switch, PQ3603G have a rating of NEMA 12? If not, what is the rating of the busplug?

No. This busplug is rated NEMA 1.


CTA-ID : 2036217
Was this helpful?
What can we do to improve the information ?