Technical FAQs

Ask a Question

Can a QO342MQ200, Nema 1, 3-phase load center, be inverted or rotated 180 degrees, so that the main circuit breaker is on the bottom of the enclosure, instead of in the top of the enclosure?

Yes, First you will need to invert, or rotate the load center 180 degrees, and then invert, or rotate the main circuit breaker 180 degrees, so that the ``OFF`` and ``ON`` `Markings` are not upside down, and will be able to be read, per the NEC Code.

CTA-ID : 2036135
Was this helpful?
What can we do to improve the information ?