Technical FAQs

Ask a Question

On a 9050JCK4 type one shot timer can you use a maintained initiating contact?

To initiate the timer the contact must be closed for at least 40ms. If a maintained initiating contact is used you must open the maintained contact at some point to reset the relay.

CTA-ID : 2036237
Was this helpful?
What can we do to improve the information ?