Technical FAQs

Ask a Question

On an EZM31200CBU main, can (3) 600 kcmil AL or CU wires be terminated per phase and neutral?

Product Features

Product Line:

Wiring accomodations

Yes. The EZM31200CBU (underground only feed) Circuit Breaker Main device is supplied with lug landing pads to accept (3) Lugs per phase and neutral (order lugs separately) and has (6) 1/2``-13 threaded studs per phase on 1 - 3/4`` centers as measured vertically and 2`` on centers as measured horizontally (NEMA Standard Spacing). Square D offers a mechanical lug kit that includes (4) ILSCO Lugs (their Cat. No.: TA6002N). Each of these lugs will accommodate (1) 3/0 AWG - 600 kcmil AL/CU wire. Order multiple Square D Cat. No.: CMELK4 lug kits. This device would require a total of 12 lugs to obtain for (3) lugs per phase, so a quantity of (4) CMELK4 kits would be needed to obtain the needed 12 lugs for this device.

CTA-ID : 2036430
Was this helpful?
What can we do to improve the information ?