Technical FAQs

Ask a Question

Can the surface cover on the J250S Series A01 enclosure be converted to a flush cover?

Cover conversion

Product Line:
Circuit Breaker Enclosures


Convert from Surface mount to flush mount cover

Yes, the surface cover for J250S Series A01 can be converted by ordering the flush cover, part number 4051585750. BUT the cover will NOT come with a Nameplate or any other labels and the Nameplate or any other labels CANNOT be ordered separately for field installation.

CTA-ID : 2036310
Was this helpful?
What can we do to improve the information ?