Technical FAQs

Ask a Question

What is the meaning of suffix 2213 on Circuit Breaker KAL361502213?

Suffix 2213 indicates that the breaker has two accessories. The first is a Normally Open (N.O.) bell alarm (Alarm contact), and the second is a 24 volt DC Undervoltage Trip unit.


CTA-ID : 2036198
Was this helpful?
What can we do to improve the information ?