Technical FAQs

Ask a Question

What is the proper torque for the lugs on the HJA36015 Powerpact breaker?

The torque values are based on wire size and are listed on the faceplate of the breaker. A 15a breaker using a wire size between #14 and #10 calls for 50 lb-in torque.

CTA-ID : 2036299
Was this helpful?
What can we do to improve the information ?