Technical FAQs

Ask a Question

What are the repair parts for a C4L200S Series M02?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053414150
Main Breaker Section Cover Assembly - 7329410550
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 7329420301
Dead Front Interior Trim Mounting Screw - 4020513001K ( This kit contains 10 screws, but only one screw is required to secure the trim)
Meter Base Assembly - 4053448450 (Includes meter base, (2) line side lugs, (4) meter jaws and (4) meter jaw blade guides and load side bussing)
Meter Jaw - (4) 4052706950 (OBSOLETE - REPLACED BY 7329794850)
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Left Line Side Lug Assembly - 4053408750
Right Line Side Lug Assembly - 4053408850
Meter Sealing Ring - 2920910001
Closing Cap - (2) ACP
Main Breaker - (2) QO type, 100A maximum
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE


CTA-ID : 2036295
Was this helpful?
What can we do to improve the information ?