Technical FAQs

Ask a Question

<br />Is the pilot light bulb included on an XY2CE device?

Pilot lights are only available on 2 N.O. - N.C. devices, and a bulb is not included. Order a bulb of the required voltage separately. BA9 incandescent bulbs are 24v = DL1CE024 , 48v = DL1CE048 and 130v = DL1CE130 .

CTA-ID : 2036167
Was this helpful?
What can we do to improve the information ?