Technical FAQs

Ask a Question

Do we ship 8941DBW08V08AP1Y68 with 2- 2 inch holes in the top and the bottom has 2- 2 inch holes and 1- 3/4 inch hole with water tight hubs?

No. The enclosure shows a total of 5 conduit entries, 2 x 1.5`` on top, 2 x 1.5`` plus 1 x .75`` on bottom. There are hubs in the enclosure for the conduit.

CTA-ID : 2036408
Was this helpful?
What can we do to improve the information ?