Technical FAQs

Ask a Question

Can we get replacement contacts for the XD4PA style joy sticks?

Issue:
Can we get replacement contacts for the XD4PA style joy sticks?
Product Line:
22MM Push Buttons
Environment:
XB4 22mm Joystick Operators
Cause:
Contacts in joystick need to be replaced.
Resolution:
Replacement contacts are available:
ZD4PA103 - Complete body and contact assembly for 2 direction
ZD4PA203 - Complete body and contact assembly for 4 direction 
Was this helpful?
What can we do to improve the information ?