Technical FAQs

Ask a Question

Can a SDSB1175C surge suppressor be mounted sideways?

Yes. There is no limitiation on the mounting of the SDSB1175C. It may be installed horizontally or vertically, etc.


CTA-ID : 2036429
Was this helpful?
What can we do to improve the information ?