Technical FAQs

Ask a Question

Is the XVBC9B or XVBC9M rated for NEMA 4X.?

The rating on the sounder is NEMA 1, 4X (indoor) and 12.


CTA-ID : 2036517
Was this helpful?
What can we do to improve the information ?