Technical FAQs

Ask a Question

What is the maximum voltage of the contacts of an 8501K Relay?<br />

The contacts are rated B300 or 300vac max (28vdc max ).


CTA-ID : 2036355
Was this helpful?
What can we do to improve the information ?