Technical FAQs

Ask a Question

Can I get a 100% rated breaker with an ET1.0I trip unit?<br /><br />

There is no way to obtain a 100% rating with a circuit breaker that has the ET1.0I trip unit. Customer has to have a version 3.0 trip unit or higher. All ET1.0I trip units are 80% rated, and mimic the response of a standard thermal magnetic breaker.




CTA-ID : 2036213
Was this helpful?
What can we do to improve the information ?