Technical FAQs

Ask a Question

Can an older obsolete Main Lug Only Split-Bus load type center be converted to a Main Breaker load center?

Issue:
Old obsolete product design features

Product Line:
QO load centers

Environment:
Convertible mains

Cause:
Application

Resolution:
No, the Older Main Lug Only split bus Load Centers were never designed or manufactured to be convertible to a Main Breaker load center. Also, split bus load centers are Obsolete, and no longer available.


CTA-ID : 2036174
Was this helpful?
What can we do to improve the information ?