Technical FAQs

Ask a Question

What is the field installable AC motor operator for the PowerPact D frame breaker?

The AC motor operators available for the PowerPact D frame breaker are:
48/60 Vac S32839
110/130 Vac S32840
208/277 Vac S32841
380/415 Vac S32845
380/480 Vac S32847

CTA-ID : 2036144
Was this helpful?
What can we do to improve the information ?