Technical FAQs

Ask a Question

Is there a blank cover available to replace the top meter socket cover in an EZMH113225 that would convert this device from a 3-Gang unit to a 2-Gang device?

Issue:
Selection

Product Line:
EZM

Cause:
Accessory selection

Resolution:
No, but a Lexan Closing Plate (Catalog Number: 29007) is available that could be used to cover the opening in the meter socket cover.

.


CTA-ID : 2036131
Was this helpful?
What can we do to improve the information ?