Technical FAQs

Ask a Question

What is the p/n for the mounting channel that goes on the wall to mount a QMB NEMA 3R enclosure 38W X 75H?

Issue:
What is the p/n for the mounting channel that goes on the wall to mount a QMB NEMA 3R enclosure 38W X 75H?

Product Line:
QMB panelboard, switchboard with QMB distribution.

Environment:
Products sold in the United States.

Cause:
Replacement parts.

Resolution:
The p/n for the channel is 80106-137-03.


CTA-ID : 2036431

Was this helpful?
What can we do to improve the information ?