Technical FAQs

Ask a Question

What is the red adjustment knob for on the NEMA ambient compensated 9065 bi-metalic overload relays?

The knob is for adjusting the thermal current range of the installed thermal units from 85 to 115%


CTA-ID : 2036346
Was this helpful?
What can we do to improve the information ?