Technical FAQs

Ask a Question

Customer asks what capacity output boost results from putting cooling fans on oil filled transformers?

Per Randy Carpenter of the MV TAG, customer was advised the following:
2500KVA and smaller=15% additional kva
2500KVA through 10,000 KVA= 25% additional kva

CTA-ID : 2036251
Was this helpful?
What can we do to improve the information ?