Technical FAQs

Ask a Question

What is the catalog number for the lug kits for Powerpact D frame circuit breaker?<br />

Field installable lug kit for the Powerpact D frame circuit breaker is 32508 which allows for 1 cable: #2-600 Cu or #2-500 Al. Qty 3 lugs per kit (one side).
The 600A lug kit 32510 will also fit the Powerpact D frame circuit breaker and allows for 2 cables: 2/0-350 Cu or 2/0-500 Al. Qty 3 lugs per kit (one side).




CTA-ID : 2036525
Was this helpful?
What can we do to improve the information ?