Technical FAQs

Ask a Question

Can I get a KAL type circuit breaker into an LA400AWK enclosure? <br /><br />

No, that enclosure will not accomodate a KAL type breaker, because of the handle mechanism; however, the LA400F, LA400S, and LA400R enclosures will accommodate a KAL breaker.


CTA-ID : 2037371
Was this helpful?
What can we do to improve the information ?