Technical FAQs

Ask a Question

Looking for a 50 ft cable for a XY2CH13150. Catalog 9007CT0201 page 33 only has one (34.4 ft) cable listed for the XY2CH.

The XY2CZ9325 which is listed for use with the XY2CE can be cut to fit from 83.7 ft to 50 ft. and is suitable for both the XY2CE and the XY2CH

CTA-ID : 2037361
Was this helpful?
What can we do to improve the information ?