Technical FAQs

Ask a Question

Where is the symbol for UL489 shown on Multi -9 breaker 60164?

The UL symbol is displayed on a sticker on the face of the breaker. It is in very small print, however. It is right over the breaker toggle handle.


CTA-ID : 2037209
Was this helpful?
What can we do to improve the information ?