Technical FAQs

Ask a Question

What is the 480V pilot light kit for a 2510K manual switch?

Use a 9999PL13 for red, or a 9999PL13G for green. If the enclosure is a NEMA 4, the kit is for replacement only as the lens in the enclosure cannot be replaced or field installed

CTA-ID : 2037208
Was this helpful?
What can we do to improve the information ?