Technical FAQs

Ask a Question

What are the dimensions for the PK32DGTA ground bar?

It is 2 3/4 inches tall from where it would mount to the enclosure to the top of Bar A. It is 6 3/4 inches wide and depth is 2 3/8 inches.


CTA-ID : 2037022
Was this helpful?
What can we do to improve the information ?