Technical FAQs

Ask a Question

On a Model 6 Motor Control Center bucket, is it possible to obtain a twin 60A fusible disconnect in one 12`` space? Similar to a QMB twin 60A fusible switch?

Issue:
On a Model 6 Motor Control Center bucket, is it possible to obtain a twin 60A fusible disconnect in one 12`` space?  Similar to a QMB twin 60A fusible switch?

Product Line:
Motor Control Center.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
This is not available. However, it is possible to use two 6`` Compact units in the 12`` space to accomplish this.


CTA-ID : 2037103

Was this helpful?
What can we do to improve the information ?