Technical FAQs

Ask a Question

What data does the Series B Micrologic trip unit communicate to Powerlogic through the CIM3F?

Powerlogic is able to get the following information from the Series B trip unit:
* A, B, C Phase True RMS Currents.
* Ground Fault Current (if ground fault option is present)
* Date and time of last trip
* Cause of last trip
* Phase currents at trip
* Ground fault current at last trip
* # of overload trips
* # of short circuit trips
* # of ground fault trips
* Breaker Type
* Sensor rating
* Plug rating
* LT settings
* ST settings
* Inst. settings
* GF settings


CTA-ID : 2036323
Was this helpful?
What can we do to improve the information ?