Technical FAQs

Ask a Question

What mounting hardware is needed when using the 9001 Type K operators to replace the obsolete 9001 Type T operators?

An 9001KIT adapter kit. This provides a washer and a gasket to seal the locating/anti-rotation hole used when mounting the 9001 Type T and provide the NEMA 4 rating.


CTA-ID : 2037313
Was this helpful?
What can we do to improve the information ?