Technical FAQs

Ask a Question

Can you add a field installable door over the I-line distribution section of a QED2 switchboard?

No you cannot. If asked for at time of order then we build that section in a NEMA 3R construction to get the door.

CTA-ID : 2037317
Was this helpful?
What can we do to improve the information ?