Technical FAQs

Ask a Question

The TVS120XR40B TVSS is intended for use on a 240/120V source. Can it be connected to a source that is 120V only?

The TVS120XR40B and TVS120XR40S are intended to be used with a 120/240V split single phase circuit. The proper device for a 120V single phase circuit is TVS120XRB or TVS120XRS.

CTA-ID : 2037298
Was this helpful?
What can we do to improve the information ?