Technical FAQs

Ask a Question

What size wire will the 9065SEO9B accept?

The 9065SEO9B power lugs have a wire range from #14 to #4 copper only, the control terminals will accept a range of #16 to #12 copper.


CTA-ID : 2036567
Was this helpful?
What can we do to improve the information ?