Technical FAQs

Ask a Question

What is the amperage range of branch breakers that can be used in a RC1624M100S?

All positions are limited to 100A maximum branch circuit breaker (#1 AWG maximum wire).


CTA-ID : 2036929
Was this helpful?
What can we do to improve the information ?