Technical FAQs

Ask a Question

Can the meter bases be swapped out on an EZMR334225 to add a lever by pass to each position, similar to an EZML334225?

No. The meter units cannot be swapped out because of the unit`s UL listing. The units cannot be changed from the functionality they have when they leave the factory. Product would then be labeled incorrectly if such a change were possible, and would not pass inspection.

CTA-ID : 2037187
Was this helpful?
What can we do to improve the information ?