Technical FAQs

Ask a Question

What is the amperage range of Service Disconnects (or main breakers) that can be used in a SC12L200S?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Main Breakers

Cause:
Application

Resolution:
This device will accept 15 to 110Amp Max and 150 to 200Amp Max. Service Disconnects ONLY. Total circuit breaker handle rating not to exceed 170A per circuit connector.


 
Was this helpful?
What can we do to improve the information ?